Analog Output
The drive has two analog outputs. You can either directly control the voltage output (AOUT#.VALUEU) or have it controlled via the action table (Set Analog Output task). Which value the analog output is driven by is selected by the AOUT#.SOURCE keyword.
|
Button or Dialog Box |
Description |
Parameter |
|---|---|---|
|
Analog Output Value (user) |
Enter the analog output value (when AOUT#.SOURCE = 0, analog output signal is determined by the user) |
|
|
Analog Output Value |
Displays the voltage that this analog output generates. |
|
| Analog Output Offset | Sets the analog output 2 offset. | AOUT#.OFFSET |
| Low Pass Filter | Enables a software-based low pass filter of the analog output value. 0 Hz is a pass-through or "disable" of this feature. | |
| Analog Output Source | Sets what drives the analog output signal. | AOUT#.SOURCE |
|
Copyright © 2018 Kollmorgen |
|